To configure
a task to start automatically:
- In Classic view,
from the iFIX WorkSpace, click the System Configuration Utility button
on the toolbar.
-Or-
In Ribbon view, on the Applications tab,
in the System & Security group, click SCU.
- On the SCU toolbox,
click the Tasks button.
- Click the browse
(...) button next to the Filename field.
- Select the desired
file and click the Open button. The selected file appears in the Filename
field.
- In the Startup Mode
area, click the Normal option button to start the task as an open window,
the Minimized option button to start the task as a minimized window, or
the Background option button to start the task in the background.
- In the Command Line
field, enter any command line parameters you may need.
- Click the Add button
to add the task to the Configured Tasks list box.
- Click the up or down
arrow buttons to move the task in the list.
- Click OK.
See Also