Configuring a Task to Run in the Background

To configure a task to run in the background:

  1. In Classic view, from the iFIX WorkSpace, click the System Configuration Utility button on the toolbar.

-Or-

In Ribbon view, on the Applications tab, in the System & Security group, click SCU.

  1. On the SCU toolbox, click the Tasks button. .
  2. Click the browse (...) button next to the Filename field.
  3. Select the desired file and click the Open button. The selected file appears in the Filename field.
  4. In the Startup Mode area, click the Background option button.
  5. In the Command Line field, enter any command line parameters you may need.
  6. Click the Add button to add the task to the Configured Tasks list box.
  7. Click OK.

 

See Also

Important Notice

You do not have the latest version of iFIX! You are missing out on the newest capabilities and enhanced security.

For information on all the latest features, see the iFIX product page.

For more information on upgrades, contact your GE Digital sales agent or e-mail GEDClientServices@gevernova.com.

For the most up-to-date documentation, go here.