Configuring an I/O Driver

To configure an I/O driver:

  1. In Classic view, from the iFIX WorkSpace, click the System Configuration Utility button on the toolbar.

-Or-

In Ribbon view, on the Applications tab, in the System & Security group, click SCU.

  1. On the SCU toolbox, click the SCADA button.
  2. Select a driver in the Configured I/O Drivers list box and click the Configure button. This starts the I/O Driver Configuration program.
  3. Enter the required information.

NOTE: You do not need to set up a SIM driver; the installation program configures it for you. For more information on the configuration program, refer to your driver documentation.

 

See Also

Important Notice

You do not have the latest version of iFIX! You are missing out on the newest capabilities and enhanced security.

For information on all the latest features, see the iFIX product page.

For more information on upgrades, contact your GE Digital sales agent or e-mail GEDClientServices@gevernova.com.

For the most up-to-date documentation, go here.