The iFIX WorkSpace has several run-time preferences, which include:
- Saving your open
documents automatically when you switch to the run-time environment. Using
this feature, you can toggle between the two environments without worrying
about saving your changes. By default, this option is disabled. If you
enable it and you want to test a change to a picture or schedule without
saving the modification, you must disable the preference before switching
to the run-time environment. If you do not, the WorkSpace automatically
saves the change.
- Displaying the
iFIX WorkSpace full-screen. This feature provides maximum screen space
for creating and displaying pictures. When you display the WorkSpace full-screen,
it hides its menu bar, system tree, and any docked toolbars. Floating
toolbars remain visible.
- Opening specific
pictures automatically when the iFIX WorkSpace starts in the run-time
environment. Use this option to define the specific files you want to
open automatically for your operators.
- Opening specific
schedules you want to open in the background. Use this option to indicate
the specific files you want the FixBackgroundServer task to load on start-up.
See Also
How Do I...