The following table outlines the steps that you must complete to deploy and configure this module for the first time.
Note: If you are deploying this module in
Step | Task | Notes |
---|---|---|
1 | Ensure that you meet the software and hardware system requirements for APM Connect. | This step is required. |
2 | On the APM Connect server, run the third-party software batch file. | This step is required |
3 | On the APM Connect Server, run the APM Connect installer. | This step is required. |
On the APM Connect Server, change and encrypt passwords. | This step is required. | |
5 | On the APM Connect server or the GE Digital APM server, install the Meridium Integration Services. | This step is required only if you are completing an on-premises deployment. |
6 | On the APM Connect server, enable Internet Explorer for APM Connect. | This step is required only if you are using Internet Explorer to access the APM Connect Administration Center. |
7 | On the APM Connect server, update PostgreSQL networking configuration. | This step is required. |
On the APM Connect server, change the PostgreSQL passwords. | This step is required. | |
On the APM Connect sever, access the APM Connect Administration Center. | This step is required. | |
On the APM Connect sever, change the APM Connect Administration Center user password. | This step is required. | |
On the APM Connect Server, validate the APM Connect Administration Center license. | This step is required only if your APM Connect Administration Center license was not validated automatically when you accessed the APM Connect Administration Center. | |
Configure the APM Connect Administration Center. | This step is required. | |
In the APM Connect Administration Center, set user permissions. | This step is required. | |
In the APM Connect Administration Center, authorize users for projects. | This step is required. | |
15 | In GE Digital APM, establish the connection from GE Digital APM to APM Connect. | This step is required only if you are completing an on-premises deployment. |
On the APM Connect Server, create a service user. | This step is required. | |
17 | On the APM Connect Server, configure logging. | This step is required only if you want to change how APM Connect logs events. |
IMPORTANT: Each of the following tasks may be required depending on the license that you have purchased and the APM Connect component that you are deploying. | ||
18 | Configure the APM Connect Administration Center for the Studio. | This step is required only if you have the APM Connect Studio license. |
19 | On the APM Connect server, install the Studio. | This step is required only if you have the APM Connect Studio license. |
20 | This step is required only if you are deploying the Data Loaders in an on-premises deployment. | |
21 | Deploy the Maximo Adapters. | This step is required only if you are deploying the Maximo Adapters. |
Deploy the SAP Adapters. | This step is required only if you are deploying the SAP Adapters. |
Copyright © 2017 General Electric Company. All rights reserved.