IMPORTANT: This step is required only if you have the APM Connect Studio license. If you are deploying APM Connect Base with a Basic or Plus License, skip this procedure and proceed to the next step in the APM Connect Base deployment workflow.
Steps
Open a web browser.
Hint: APM Connect is most compatible with Google Chrome or Mozilla Firefox web browsers. It is not recommend using Internet Explorer to access the APM Connect Administration Center.
In the Menu pane, in the Settings section, select the Configuration tab.
The Configuration pane appears.
Select the Svn (7 Parameters) group to expand the workspace.
According to the following table, enter the necessary parameters.
Parameter | Description | Recommended or Default Value |
---|---|---|
Server location URL | URL location of the SVN server. | http://localhost/svn/MIAPMINT |
Username | SVN user name created to use in the APM Connect Administration Center when installing the SVN server. | APM |
Password | SVN password created to use in the APM Connect Administration Center when installing the SVN server. | Connect |
Commit Log Pattern | SVN commit log according to your log format convention. | {0} |
Library location URL | URL location of the SVN external libraries directory downloaded with the Studio. | Not Required |
Library username | User name of the SVN user that has access to the libraries directory. | Not Required |
Library password | Password of the SVN user that has access to the libraries directory. | Not Required |
The default parameters are configured as shown in the following image.
According to the information in the following table, enter the necessary parameters.
Parameter | Description | Recommend or Default Value |
---|---|---|
Host | The IP address of the CommandLine. | localhost |
Port | The port number on which the CommandLine is queried. | 8002 |
Job generation folder | The path to the folder where Jobs are generated. | <root:>\APMConnect\Utilities\cmdline\generationCache |
User component path | The path to the folder where user components are stored. | <root:>\APMConnect\Utilities\cmdline\custom_components |
The default parameters are configured as shown in the following image.
What's Next?
Copyright © 2017 General Electric Company. All rights reserved.