Import Adapter Jobs

Note: This step is needed only if the adapter jobs were not imported when you ran the APM Connect installer.

A job is used to extract information from the source and push it into GE Digital APM. Before you can initiate a job using the APM Connect Administration Center, you must first load the jobs into the APM Connect Administration Center. This is accomplished by importing the jobs from a .zip file. This topic describes how to import jobs into the APM Connect Administration Center.

Steps

  1. In the Menu pane, in the Conductor section, select the Job Conductor tab.
  2. On the Job Conductor toolbar, select Add.

    The Execution task pane is activated.

  3. In the Execution task pane, in the Label box, enter a label for the job.

  4. In the Description box, enter a description for the Job.

  5. Select the Active check box.

  6. In the Job section, select .

    The Import generated code window appears.

  7. Select Browse, and then navigate to the folder containing the updated jobs package.

  8. Depending on the type of deployment, select the files that contains the job based on the following table.

    Note: You must import every job, or run the respective wrapper job, in the table for the respective deployment.

  9. On the Import generated code window, select Launch upload.

    The Project, Branch, Name, Version, and Context boxes are automatically populated with appropriate values.

  10. In the Execution Server list, select the server on which the task should be executed.
  11. Select Save.

    The Adapter Job is imported into the APM Connect Administration Center.

  12. Repeat steps 2-12 for every job.

    Each Job is automatically categorized into the correct project.

What's Next?

Copyright © 2017 General Electric Company. All rights reserved.