A standard gas cylinder is a pressure vessel that stores a mixture of gases of known composition. It is used to calibrate single and multi-component analyzers. The details of a standard gas cylinder and its components are stored in a Standard Gas Cylinder record and Standard Gas Component records, respectively. You must create these records before you calibrate single or multi-component analyzers. Note that for each component in the cylinder, you must create one Standard Gas Component. A Standard Gas Cylinder is linked to each Standard Gas Component through the Has Component relationship.
While creating a Calibration Template for a single or multi-component analyzer, you can link a Standard Gas Cylinder to the template. The Meridium Enterprise APM system creates one Calibration Template Detail record for each component of the cylinder.
Copyright © 1993-2015 Meridium, Inc. All rights reserved.