Calibration Records

Calibration records store information about the calibration event that you have performed either manually or using a device. Based on the type of calibration that you have performed, the following Calibration records are created:

The following table provides an alphabetical list and description of the fields that exist for the aforementioned Calibration families. The information in this table reflects the baseline state and behavior of these fields. This list is not comprehensive.

Field Data Type Description Behavior and Usage
Calibration Approval By Character The name and User ID of the user who approved the calibration. This field contains a list of user names. You can select the appropriate user from the list.
Calibration Closed Logical Indicates whether or not the calibration even is closed. By default, this field is cleared.

If you select this check box:

  • All the fields in the Calibration are disabled.
  • The date and time on which you select the check box is used to populate the Last Date field in the Calibration Task whose ID appears in the Tasks Addressed field.
  • If your database has been configured correctly, a Task Execution record will be created and linked to the Calibration and the Calibration Task whose Entity ID appears in the Tasks Addressed field.
  • The value in the Date Executed field in the Task Execution record will be set automatically to the date that the Calibration Close check box was selected. This field is enabled only for Super Users and members of the Calibration Administrator Security Group.
Calibration End Date Date The date on which you have completed the calibration. This field is populated with the current date and time. You can modify this value if needed.
Calibration Error Limit Number A number indicating the maximum percentage of acceptable error before the calibration is considered to be failed.

This field is populated with the value stored in the Max Error Limit field of the Calibration Template that is linked to this Calibration. You can modify this value if needed.

If the value in the Calibration Type field is anything other than Analog-Manual or the Calibration Close check box is selected, this field is disabled.

Calibration Start Date Date The date on which you have started calibrating the asset. This field is populated with the current date and time. You can modify this value if needed.
Calibration Strategy Character The number of test points and the direction of the input signal that will be recorded for the calibration.

This field is populated with the value in the Calibration Strategy field of the Calibration Template that is linked to this Calibration.

Calibration Task ID Character The ID of the Calibration Task that is linked to this Calibration.

This field contains a list of Calibration Tasks that are linked to the Equipment or the Calibration Template that you have selected.

If there is only one Calibration Task in the list, this field is disabled and populated with the ID of that Calibration Task.

After you select a Calibration Task, a few other fields in the Calibration will be populated with data from the specified Calibration Task.

Calibration Technician Character The name of the person who is responsible for performing the calibration.

If you perform a manual calibration, this field is populated with the name and User ID of the user who created the record. You can, however, modify this value by selecting a user from the list.

Calibration Template Number The ID of the Calibration Template to be linked to the Calibration.

This field contains a list of Calibration Templates that are linked to the Equipment or the Calibration Task that you have selected.

If there is only one Calibration Template in the list, this field is disabled and populated with the ID of that Template.

After you select a Calibration Template, a few other fields in the Calibration record will be populated with data from the specified Calibration Template.

Calibration Type Character The type of calibration event.

This field is disabled and populated with the value, Analog - Manual.

Comments Character Any comments on the calibration that you have performed. None
Cylinder Expiry Date Date The expiry date of the standard gas cylinder. This field is disabled and populated based on your selection in the Cylinder ID field.
Cylinder ID Character The ID of the Standard Gas Cylinder that is used to perform the calibration. None
Engineering Units Error Limit Character The maximum amount of error in engineering units that is allowed before a calibration event is considered failed.

This field appears only on the Calibration, Discrete datasheet below the column labeled % of Scale. This field is disabled and populated with a default value from the Calibration Setup Defaults record.

  • If the Error Assessment field in the Calibration Setup Defaults record contains the value Engineering Units, this field is enabled and populated with a default value. If you modify this value, the value in the Error Limit field will be updated automatically. You can enter a value between 0 and 100.
  • If the Error Assessment field in the Calibration Setup Defaults record contains the value Percent of Range, this field is disabled and calculated as follows:

    (<Max Error Limit>/100) x (<URV> - <LRV>)

    ...where:

    • <Max Error Limit> is the value in the Max Error Limit field.
    • <URV> is the value in the Primary Input Range URV field.
    • <LRV> is the value in the Primary Input Range LRV field.
Equipment ID Character The ID of the equipment that you have calibrated. This field contains a button, which you can select to search for an Equipment. After you select an Equipment, the Calibration Template and the Calibration Task ID fields display a list of templates and tasks linked to the Equipment respectively.
Equipment Manufacturer Character The manufacturer of the equipment that you have calibrated. This field is populated with the value stored in the Manufacturer field in the Equipment that is linked to the Calibration. You can modify this value if needed.
Equipment Model Number Character The model number of the asset that you have calibrated. This field is populated with the value stored in the Model Number field in the Equipment that is linked to the Calibration. You can modify this value if needed.
Equipment Serial Number Character The serial number of the asset that you have calibrated. This field is populated with the value stored in the Equipment Serial Number field in the Equipment that is linked to the Calibration. You can modify this value if needed.
Equipment Short Description Character A brief description of the asset that you have calibrated. This field is populated with the value stored in the Equipment Short Description field in the Equipment that is linked to the Calibration. You can modify this value if needed.
Equipment Type Character The type of the asset that you have calibrated.

This field is populated with the value stored in the Equipment Type field in the Equipment that is linked to the Calibration. You can modify this value if needed.

Error Assessment Character The measurement type that you will use in case of a discrete calibration.

This field appears on the Calibration, Discrete datasheet and contains the following values:

  • Percent of Range: When this value is selected, the Error Limit field is enabled, and the Engineering Units Error Limit field is disabled.
  • Engineering Units: When this value is selected, the Engineering Units Error Limit field is enabled, and the Error Limit field is disabled.
Event End Date Date The date on which the calibration event was completed.

On the datasheet, this field appears as a text box labeled Calibration End Date.

If you perform a manual calibration, this field is populated with the date and time that the Calibration record was created. You can modify this value if needed.

Event ID Character The ID of the calibration event. This field is disabled and populated with a default value.
Event Long Description Character Additional comments about the calibration event. None
Event Start Date Date The date on which the calibration event is initiated. This field is populated with the date and time that the Calibration was created. You can modify this value if needed.
Input Characteristic Curve Character The characteristics of the input signal to the instrument that you are calibrating.

This field contains the following values:

  • Linear
  • Percent
  • Square Root
  • None
Instrument Manufacturer Character The manufacturer of the equipment that you have calibrated. This field is populated with the value stored in the Equipment Manufacturer field in the Equipment that is linked to the Calibration. You can modify this value if needed.
Instrument Model Number Character The model number of the equipment that you have calibrated. This field is populated with the value stored in the Equipment Model Number field in the Equipment that is linked to the Calibration. You can modify this value if needed.
Instrument Serial Number Character The serial number of the equipment that you have calibrated. This field is populated with the value stored in the Equipment Serial Number field in the Equipment that is linked to the Calibration. You can modify this value if needed.
Location ID Character The physical location where you have performed the calibration. None
Location Short Description Character A description of the location where you have performed the calibration. None
Maintenance Type Character The type of maintenance performed by this calibration event. By default, this field contains the value Scheduled.

This field contains the following values:

  • Scheduled
  • Repair
  • Unscheduled
  • New Installation
Off Line Duration Number A number representing the amount of time in hours that passed between the time the calibration was initiated and the time that it was completed. None
Output Characteristic Curve Character The type of output signal to the piece of equipment being calibrated.

This field contains the following values:

  • Linear
  • Percent
  • Square Root
  • None
Overall AF Error Max Number A number that corresponds to the highest error value recorded from all the As Found values in all existing records in the current family. This field is disabled and populated with the highest error value from all the As Found error values. If the calculated value contains more than six digits, it will be rounded.
Overall AF Pass/Fail Character A value that indicates whether the calibration passed or failed based on whether the As Found values fall within the range of values specified in the record. This field is disabled and populated. If the value in the Overall AF Error Max field is greater than the value stored in the Calibration Error Limit field, this value is Fail. Otherwise, this value is Pass.
Overall AL Error Max Number The highest error value recorded for all the As Left values in all the existing records in the Calibration family. This field is disabled and populated with the highest error value from all the As Left error values. If the calculated value contains more than six digits, it will be rounded.
Overall AL Pass/Fail Character A value that indicates whether the calibration passed or failed based on whether the As Left values fall within the range of values specified in the Calibration. This field is disabled and populated. If the value in the Overall AL Error Max field is greater than the value stored in the Calibration Error Limit field, this value is Fail. Otherwise, this value is Pass.
Scheduled Date Date The date on which the calibration is scheduled to be performed. None
Test Equipment Cal. Expire <Number> Date The date on which the certification of the test equipment expires. This field appears as a text box labeled Calibration Expire and is populated with the value stored in the Next Certification field in the Test Equipment linked to this Calibration.
Test Equipment ID No <Number> Character The ID of the Test Equipment that is linked to the Calibration.

This field appears as a text box labeled ID No.

  • If you select a Test Equipment that is certified, this field will be shaded green.
  • If you select a Test Equipment that is not certified, a message appears indicating that the Test Equipment is out of certification, and the field will be shaded red.

If you try to select the same Test Equipment more than once in the same Calibration, an error message appears.

Test Equipment Last Cal. <Number> Date The date on which the test equipment was most recently certified. This field appears as a text box labeled Last Calibration Date and is populated with the value stored in the Last Certification Date field in the Test Equipment that is linked to the Calibration.
Test Equipment Manufacturer <Number> Character The manufacturer of the test equipment.

This field appears as a text box labeled Manufacturer and is populated with the value stored in the Manufacturer field in the Test Equipment that is linked to this Calibration.

Test Equipment Model Number <Number> Character The model number of the test equipment.

This field appears as a text box labeled Model Number and is populated with the value stored in the Model Number field in the Test Equipment that is linked to the Calibration.

Test Equipment Serial Number <Number> Character The serial number of the test equipment.

This field appears as a text box labeled Serial Number and is populated with the value stored in the Serial Number field in the Test Equipment that is linked to the Calibration.

Test Equipment Status <Number> Character The certification status of the test equipment. This field appears as a text box labeled Status and is populated with the value stored in the Certification Status field in the Test Equipment that is linked to the Calibration.
WO Reference Character The work order number associated with the calibration event. None

Copyright © 1993-2015 Meridium, Inc. All rights reserved.