What If Analysis Workflow

Using the Hazards Analysis module, you can conduct the following types of Hazards Analyses:

This workflow provides the basic, high-level steps for using this module. The steps and links in this workflow do not necessarily reference every possible procedure. For more procedures, see the links in the Related Information section.

Conducting a What If Analysis includes completing the following steps:

  1. Create a Hazards Analysis, which stores the details of the What If Analysis that you want to perform, including the start and end dates for the analysis.
  2. Identify the Systems/Nodes in which the hazardous scenario originates.
  3. Define components, which includes identifying the following items:

  4. Assess the unmitigated and mitigated risks.
  5. Link Assets to each System/Node in the What If Analysis.
  6. Define the Hazards Analysis team who will conduct the analysis.
  7. Link the Hazards Analysis to a Reference Document, which contains the reference material relevant to the analysis.
  1. Propose a Recommendation for actions that should be taken to mitigate the risk in that scenario.

Copyright © 1993-2015 Meridium, Inc. All rights reserved.