Create a Failure Mode

Steps

  1. Access the RCM Module Overview page.
  2. Select the analysis containing the Functional Failure for which you want to create a Failure Mode.

    In a new tab, the Analysis Details (Analysis Details) workspace for the selected analysis appears, displaying the Analysis Overview (Analysis Overview) section.

  3. In the left pane, select the function that contains the Functional Failure for which you want to create a Failure Mode.

    In the left pane, the Functional Failures for the selected function appear.

  4. In the left pane, select the Functional Failure for which you want to create a Failure Mode.

    The workspace for the selected Functional Failure appears.

  5. In the left pane, select , and then select Add Failure Mode (Add Failure Mode).

    The workspace for the new Failure Mode appears, displaying the Failure Modes (Failure Modes) section.

  6. As needed, enter values in the available fields.
  7. Select .

    The Failure Mode is saved.

Copyright © 1993-2015 Meridium, Inc. All rights reserved.