Overview of the RCM Data Model

The following table provides a summary of the entity families and relationship families that are used to develop an RCM Analysis.

Records in this entity family:

...Can be linked to records in this entity family:

...Through a relationship definition on this relationship family: 

RCM FMEA Analysis

RCM Function

Has RCM Function

RCM Function

RCM Functional Failure

Has RCM Functional Failure

RCM Functional Failure

RCM FMEA Failure Mode

Has RCM FMEA Failure Mode

RCM FMEA Failure Mode

RCM FMEA Failure Effect

Has RCM FMEA Failure Effect

RCM FMEA Failure Effect

RCM FMEA Recommendation

Has RCM FMEA Recommendation

In addition, the following families and relationships are used by RCM by not within the analysis tree itself.

Records in this entity family: ...Can be linked to records in this entity family: ...Through this relationship: Purpose
RCM FMEA Analysis Human Resource Has RCM FMEA Team Member Facilitates the construction of the RCM Analysis Team Members list. Through this relationship, Human Resource records are linked directly to the RCM FMEA Analysis record.
RCM FMEA Analysis RCM FMEA Asset Has RCM FMEA Asset Facilitates the construction of the RCM equipment list. In this way, the RCM FMEA Asset records are linked directly to the RCM FMEA Analysis record. Note, however, that RCM FMEA Asset records do not appear in the analysis tree of an RCM Analysis.
RCM FMEA Analysis RCM FMEA Task Has Tasks Allows Task records generated from Recommendation records to be linked to the RCM FMEA Analysis record for which the recommendation was created. Note that in the current version of Meridium Enterprise APM, RCM FMEA Task records cannot be created from RCM FMEA Recommendation records. Instead, RCM FMEA Recommendation records can be used to create Action records in ASM. This relationship still exists, however, to support legacy RCM FMEA Task records.
RCM FMEA Recommendation RCM FMEA Task Has Tasks Allows RCM FMEA Recommendation records to be linked to RCM FMEA Task records that are generated from those recommendations. Note that in the current version of Meridium Enterprise APM, RCM FMEA Task records cannot be created from RCM FMEA Recommendation records. Instead, RCM FMEA Recommendation records can be used to create Action records in ASM. This relationship still exists, however, to support legacy RCM FMEA Task records.
RCM FMEA Asset Asset Strategy Template Has Strategy Facilitates the promotion of RCM FMEA Asset records to Asset Strategy records via Recommendation Management. This link is established when an RCM FMEA Analysis is linked to a physical or "virtual" piece of equipment or location for which you have defined Recommendation records.
RCM FMEA Asset RCM FMEA Task Has Tasks

Allows RCM FMEA Asset records to be linked to RCM FMEA Task records. This link is established only when a Task record is generated from a recommendation where the related RCM FMEA Asset record (i.e., the RCM FMEA Asset record that is linked to the RCM FMEA Analysis record) is not linked to an Equipment or Functional Location record.

Note that in the current version of Meridium Enterprise APM, RCM FMEA Task records cannot be created from RCM FMEA Recommendation records. Instead, RCM FMEA Recommendation records can be used to create Action records in ASM. This relationship still exists, however, to support legacy RCM FMEA Task records.

RCM FMEA Asset Task History Has Task History Facilitates the rejection of RCM FMEA Task records that are linked to RCM FMEA Asset records. When you reject an RCM FMEA Task record, a Task History record is created and linked to the RCM FMEA Asset record through the Has Task History relationship.
RCM FMEA Asset Task History Has Task History Facilitates the rejection of RCM FMEA Task records that are linked to RCM FMEA Asset records. When you reject an RCM FMEA Task record, a Task History record is created and linked to the RCM FMEA Asset record through the Has Task History relationship.
RCM FMEA Analysis Has Templates RCM FMEA Template Facilitates the creation of RCM Templates.
RCM FMEA Asset Has Templates RCM FMEA Template Facilitates the creation of RCM Templates.
RCM Function Has Templates RCM FMEA Template Facilitates the creation of RCM Templates.
RCM Functional Failure Has Templates RCM FMEA Template Facilitates the creation of RCM Templates.
RCM FMEA Failure Mode Has Templates RCM FMEA Template Facilitates the creation of RCM Templates.
RCM FMEA Failure Effect Has Templates RCM FMEA Template Facilitates the creation of RCM Templates.
RCM FMEA Recommendation Has Templates RCM FMEA Template

Facilitates the creation of RCM Templates.

RCM FMEA Recommendation Mitigates Risk Risk Assessment Allows you to determine how a recommendation mitigates a risk.

Note that also the following families are related to the RCM FMEA Template family through the Has Templates relationship to facilitate the creation of RCM Templates:

Copyright © 1993-2015 Meridium, Inc. All rights reserved.