RCM Analysis State Configuration

This topic describes the different analysis states in an Reliability Centered Maintenance (RCM) analysis configuration.

By default, the following baseline State Configuration exists for the RCM Analysis family.

Initial State

The Draft state is the initial state of all new RCM Analysis records.

Datasheet Configuration

By default, no states and operations will appear on the datasheet when you are viewing an RCM FMEA Analysis record in RCM, FMEA, the Record Manager, or the Bulk Data Form.

Reserved States and Operations

By default, no states or operations displayed in the preceding diagram are reserved. This means that you can remove or modify any of these states or operations. You can also add your own states and operations to the State Configuration.

State Configuration Roles

By default, the MI RCM User State Configuration Role is assigned to all states in the RCM FMEA Analysis State Configuration. If required, you can assign other State Configuration Roles to any state.

Copyright © 1993-2015 Meridium, Inc. All rights reserved.