Access the Source Data for a Reliability Distribution Analysis

You can access the source data only if the analysis is based on a query or a dataset.

Steps

  1. Access a Reliability Distribution Analysis for which you want to view the source data.
  2. In the left pane, select the Probability Plot tab.

    The Probability Plot appears in the workspace.

    Probability Plot

    Note: You can also view data for a plot via the Failure Rate Plot , PDF Plot, CDF Plot, or Failure Probability.

  3. In the upper-right corner of the workspace, select Analysis Data, and then select Go To Source.

    The fields on the page that appears display the analysis data associated with the selected Reliability Distribution Analysis and correspond to values that were used to create the analysis.

Copyright © 1993-2015 Meridium, Inc. All rights reserved.