Production Loss Regions Section

The Production Loss Regions section of the Production Analysis report contains a grid that displays information that is stored in the Production Losses records that are linked to the Production Analysis record. Each row in the grid represents one Production Losses record that is linked to the Production Analysis record.

Production Loss Regions Section

The following table lists each column in the grid in the Production Loss Regions section and the corresponding Production Losses record field whose data is displayed in the report.

Column Production Losses Field
Name

Losses Type

Region Start

Area Start

Region End

Area End

Quantity Production Losses
Cost

Losses Cost

Copyright © 1993-2015 Meridium, Inc. All rights reserved.