Access Production Analysis Report

Steps

  1. Access a Production Analysis whose report you want to access.
  2. In the left pane, select the Report tab.

    The Report workspace for the selected analysis appears, displaying the Master Report section.

    Reports Tab

  3. In the Master Report section, select the Production Analysis Report link.

    The Production Analysis report appears in a new tab.

    Production Analysis Report

    By default, the report contains the following sections:

    Note: By default, the report contains all the sections listed above. You can, however, exclude a section from the report. To do so, in the upper-right corner of the page, select Refresh. On the Enter Parameter Values window that appears, set the the value of a field to False to exclude the corresponding section from the report, and then select Done.

    You can also view report for a different Production Analysis. To do so, provide the Analysis ID in the Entity Key box for the analysis for which you want to view a report, and then select Done.

Copyright © 1993-2015 Meridium, Inc. All rights reserved.