The baseline Meridium Enterprise APM database includes the Production Analysis Report, which you can use to view a summary of the results of a Production Analysis.
The Production Analysis Report is built from the following Catalog items:
Throughout this documentation, we refer to the main report, the subreport, and the supporting queries collectively as the Production Analysis Report.
The Production Analysis report contains a prompt on the ENTY_KEY field in the Production Analysis family. When you run the Production Analysis report via the Production Analysis module, the ENTY_KEY of the Production Analysis record associated with the current analysis is passed automatically to the prompt, and the results for the current Production Analysis are displayed. If you run the main report or any of the queries in the preceding list directly from the Catalog, however, you will need to supply the ENTY_KEY of a Production Analysis record manually to retrieve results. The subreport (i.e., Catalog item SubreportProductionAnalysis) cannot be run directly from the Catalog.
Copyright © 1993-2015 Meridium, Inc. All rights reserved.