About RBI Recommendations

Note: Unless otherwise specified, the content in this topic is applicable to both RBI 580 and RBI 581 methodologies.

An RBI Recommendation stores information about actions that should be performed to help mitigate the risk associated with a degradation mechanism. Each RBI Recommendation record is linked to:

Generating Recommendations

Meridium Enterprise APM generates Recommendations for:

In RBI 581, you can generate Recommendations based on the policies that are mapped to the RBI Strategies only if:

These Recommendations are:

If the methodology is RBI 580, Recommendations are generated for Degradation Mechanisms that are related to all RBI 581 Damage Mechanism Methodologies. However, If the methodology is RBI 581, Recommendations are generated for Degradation Mechanisms that are related only to the following Damage Mechanism Methodologies:

You can promote these Recommendations to Asset Strategy Management (ASM), where they are converted into Inspection Tasks.