IMPORTANT: All PRD and Pipeline Analyses function in the same way as RBI Analyses unless otherwise noted.
A PRD Analysis can only be created for PRD Components that have protected RBI Components or an asset. If the PRD Component is protecting RBI Components, then one of the RBI Components should have an active analysis. A PRD Analysis will also inherit the PDMs from the PRD Component.
If the component is an RBI Pipeline Segment, the created analysis will be a Pipeline Analysis.
Below the graph, select .
A new analysis is created, and the Analysis workspace for the new analysis appears, displaying the Analysis Details section.
Note: When an analysis is created, the Consequence Evaluations and Degradation Mechanisms corresponding to the Potential Degradation Mechanisms linked to the selected component are also created.
Copyright © 1993-2015 Meridium, Inc. All rights reserved.