Data Model

Rounds leverages the fundamental Meridium Enterprise APM entity and relationship family infrastructure for storing data in the Meridium Enterprise APM database. The data that is stored in the Meridium Enterprise APM database can be transferred to a mobile device, where you can record readings and create recommendations. Those readings and recommendations can then be transferred to the Meridium Enterprise APM database, where they will be converted into records.

When you are working with records in Rounds, it is helpful to visualize the data model illustration.

In the following illustration:

Copyright © 1993-2015 Meridium, Inc. All rights reserved.