The following System Code Tables are used by Rounds:
|
Table ID |
Table Description |
Function |
|---|---|---|
|
MI_RECOMMENDATION_TYPE |
CORE, Recommendation Type |
Used to populate the Recommendation Type list in Recommendation records. Note that the Recommendation Type field is not included on the baseline OPR Recommendation datasheet. |
|
MI_FDC_STATUS_TYPE |
Status type for Checkpoint families |
None |
|
MI_OPR_MEAS_LOC_TYPE |
List of Measurement Location types |
Used to populate the Measurement Location Type list in Measurement Location records and the Type list on the Operator Rounds Allowable Values page. |
|
MI_TASK_TYPE_REFERENCE |
CORE, Reference values to limit task type lists when creating tasks |
Used to populate the Task Type field in Checkpoint Task records. |
|
Reading Status |
Reading Status |
Used to populate the Status field in Reading records. |
|
Route Status |
Route Status |
Used to populate the Status field in Route History records. |
|
UOME |
Units of measure |
Used to populate the Unit of Measure list in Measurement Location records. |
Copyright © 1993-2015 Meridium, Inc. All rights reserved.