About Common Cause Failure

A common cause failure is a failure or condition within a plant that can affect the operation of multiple instrumented functions. SIF Common Cause Failures must be linked to at least two Instrumented Functions. In other words, for every SIF Common Cause Failure, there will be at least two Instrumented Function records that represent the instrumented functions that are affected by the common cause failure defined in the SIF Common Cause Failure record.

You can manage SIF Common Cause Failure records via the Common Cause Failures section of the Instrumented Function. Using the Common Cause Failures section, you can specify the common cause failures that exist for the current instrumented function and other instrumented functions that are defined in the Meridium Enterprise APM database. More specifically, to define a common cause failure, you will need to:

The following illustration shows the records that will exist for a given common cause failure scenario.

Copyright © 1993-2015 Meridium, Inc. All rights reserved.