Create an Instrumented Function

Steps

  1. Access the SIL Analysis for which you want to create an Instrumented Function.

  2. In the left pane, select , and then select Create New.

    A blank datasheet for the Instrumented Function appears.

    The blank datasheet of an Instrumented Function

  3. As needed, enter values in the available fields.
  4. In the lower-right corner of the datasheet, select Save.

    The Instrumented Function is created.

What's Next?

Copyright © 1993-2015 Meridium, Inc. All rights reserved.