Create a Recommendation

Steps

  1. Access the Instrumented Function for which you want to create a Recommendation.
  2. In the upper-right corner of the page, select .

    The Recommendations pane appears, displaying a list of Recommendations linked to the Instrumented Function.

    The Recommendations pane

  3. In the upper-left corner of the pane, select .

    A blank datasheet of the Recommendation appears.

    The blank datasheet of a Recommendation

  4. As needed, enter values in the available fields, and then in the upper-right corner of the datasheet, select .

    The Recommendation is created.

    Note: See the Recommendation Management Workflow section of the documentation for additional options when working with Recommendations.

Results

Copyright © 1993-2015 Meridium, Inc. All rights reserved.