On the top navigation bar, select .
The Asset Hierarchy appears.
In the Asset Hierarchy, select the Functional Location you want to view in the Thickness Monitoring Overview workspace.
Below the workspace heading, select the Strategy tab, and then in the Thickness Monitoring row, select TM Assets.
The TM page appears, displaying the Thickness Monitoring Overview workspace.
Note: The Assets tab and section only list assets that have Corrosion Analysis Settings. If you want to include another asset, you will first need to create Corrosion Analysis Settings for that asset.
The tabs at the top of the page summarize the number of TM assets and their corresponding functions in various categories. You can select a tab to view one of the following lists:
The Thickness Monitoring Overview workspace also contains the following graphs and charts:
Optionally, if you have configured Thickness Monitoring to link Functional Locations directly with TMLs and TML Groups, in the upper-right corner of the workspace, you can select to open the Functional Location in the Analysis Overview workspace.
Copyright © 1993-2015 Meridium, Inc. All rights reserved.