Archive an Asset Corrosion Analysis

Steps

  1. Access the Analysis Overview for the asset that contains the Corrosion Analysis that you want to archive.

    Note: Corrosion Analyses can only be archived on the asset level.

  2. In the upper right corner of the workspace, select , and then select Archive Analyses.

A message appears, confirming that you want to archive the selected Corrosion Analysis.

  1. Select Yes.

The Asset Corrosion Analyses for the asset, and all TML Groups linked to the asset, are archived.

Results

Copyright © 1993-2015 Meridium, Inc. All rights reserved.