Access the Analysis Overview

The Analysis Overview can be accessed via an asset, a TML Group, or a Thickness Measurement Location (TML).

Steps

  1. Access the Thickness Monitoring Overview for the Functional Location that contains the asset, TML Group, or TML whose Analysis Overview you want to access.

  2. In the workspace heading, select the Assets tab.

    The Assets section appears, displaying a list of assets with Corrosion Analysis Settings that are contained in the Functional Location.

  3. In the list, in the Asset ID column, select an asset.

    The Analysis Overview workspace appears.

    Note: The Analysis Overview workspace for a TML Group displays the same tabs and sections.

    Tip: To view and modify the datasheet for the selected asset or TML Group, in the workspace heading, select the Details tab.

    If you want to access the Analysis Overview for a:

  4. In the left pane, select a TML Group.

    The Analysis Overview workspace appears.

  5. In the left pane, select a TML.

    The Analysis Overview workspace appears.

    Tip:

    • To view and modify the datasheet of the selected TML, in the workspace heading, select the Details tab.
    • To view the Asset or TML Corrosion Analysis datasheet for the selected asset, TML Group, or TML, select the Details tab within the Analysis Output section.

Results

When you access the Analysis Overview, the Summary subsection of the Analysis Output section appears, displaying a summary of the Asset or TML Corrosion Analysis for the selected asset, TML Group, or TML.

From the Analysis Overview workspace for an asset or TML Group, you can also:

From the Analysis Overview workspace for a TML, you can also:

Copyright © 1993-2015 Meridium, Inc. All rights reserved.