Calculate a Bulk Analysis

When you calculate a bulk analysis, the following analyses will be updated:

Steps

  1. Access the Thickness Monitoring Overview for the functional location that contains the assets that you want to include in a bulk analysis.

  2. Select the Assets tab.

    The Assets section appears.

    Note: Optionally, you can select the Assets Requiring a Calculation tab to see which assets require calculation, and then follow the same procedures described below.

  3. Select the check boxes corresponding to the assets that you want to analyze.

    The Bulk Analyze button is enabled.

  4. Select Bulk Analyze.

    The Bulk Analyze disclaimer appears.

  5. Select Yes.

    The Bulk Analyze window appears, displaying a list of the selected assets.

    Asset and TML Corrosion Analyses are calculated.

    In the box at the bottom of the window, a log of the operation appears.

    The Calculation Completed status appears beside all records for which the operation was successful.

    If the Validation Failed status appears beside an analysis, proceed to step 6. Otherwise, skip to step 7.

  6. In the list, select the record whose log you want to view.

    A log of the operation associated with that record appears, along with an explanation of any errors.

  1. Select Done.

Copyright © 1993-2015 Meridium, Inc. All rights reserved.