Create a Thickness Measurement Location (TML)

Steps

  1. Access the Analysis Overview for the asset or TML Group for which you want to create a new TML.

  2. In the left pane, select , and then select TML.

    The Create TML window appears.

  3. In the TML ID box, enter a unique TML ID.

  4. In the Analysis Type box, select the type of analysis that you want to create.

    If you have defined additional required fields for TMLs, proceed to the next step. Otherwise, skip to step 7.

  5. Select Next.

    The TML datasheet appears.

  6. In the required fields, enter the necessary values.
  7. Select Done.

    The new TML is created, and the TML Overview workspace appears.

Results

Copyright © 1993-2015 Meridium, Inc. All rights reserved.