Relocate a Thickness Measurement Location (TML)

Relocate TMLs is used to move TMLs from a source asset or TML Group to a different target asset, or to a TML Group or subcomponent linked to that target asset. If you need to move TMLs to or between subcomponents linked to the same asset, use Organize TMLs.

Steps

  1. Access the Analysis Overview for the asset the TMLs you want to relocate.

  2. Select , and then select Relocate TMLs.

    The Relocate TMLs workspace appears.

  3. In the list, select the check boxes corresponding to the TMLs that you want to relocate.

    Note: If you do not see the TMLs that you expect, or want to limit the list, in the upper-left corner of the workspace, confirm the setting in the Analysis Type list, and whether the Active TMLs Only check box is selected.

  4. Select Select an Asset.

    The Select Target window appears.

  5. In the Asset Hierarchy, select the asset to which you want to relocate the TMLs.

    In the Selected Item box, the Asset ID for the asset appears. In the Available Subcomponents box, a list of linked subcomponents appears.

  6. If you want to relocate the TMLs to a subcomponent, such as a TML Group, in the Available Subcomponents box, select the subcomponent to which you want to relocate the TMLs.
  7. Select Done.

    The TMLs are relocated to the selected asset or subcomponent.

    Results

    The analyses of the affected assets and subcomponents are recalculated.

Copyright © 1993-2015 Meridium, Inc. All rights reserved.