Renew a Thickness Measurement Location (TML)

Steps

  1. Access the Analysis Overview for the asset or TML Group that contains the TMLs that you want to renew.

  2. Select , and then select Renew TMLs.

    The Renew TMLs window appears, displaying a list of the TMLs linked to the asset or TML group.

  3. In the list, select the check boxes corresponding to the TMLs that you want to renew.

    Note: If you do not see the TMLs that you expect, or want to limit the list, in the upper-left corner of the window, confirm the setting in the Analysis Type box, and whether the Active TMLs Only check box is selected.

  4. Select Renew TMLs.

Copyright © 1993-2015 Meridium, Inc. All rights reserved.