IMPORTANT: Do not switch application tabs (i.e., the tabs within Meridium Enterprise APM) while using the Measurement Data Entry workspace. To avoid losing data, you must save entered measurements before switching tabs.
Access the Analysis Overview for the asset or TML Group for which you want to record Thickness Measurements.
In the workspace heading, select .
The Measurement Data Entry workspace appears, displaying a list of TMLs.
In the common measurement data section, enter values into the Measurement Taken Date, Measurement Taken By, and Temperature boxes.
Note: If you have customized the common measurement data section, there may be additional boxes available.
In the data entry grid, enter values into the Readings cell for each TML.
Each time you enter a value into a Readings cell, the other cells in the row that correspond to the boxes in the common measurement data section are populated with the values that you entered in step 3.
If the data entry grid contains a TML that requires you to enter multiple readings, proceed to the next step. Otherwise, skip to step 7.
In the Readings cell corresponding to a TML that requires multiple readings, select .
The Readings window appears.
In each box, enter a value, and then select OK.
The Measurement Data Entry workspace appears. The Readings cell corresponding to the TML that you selected in step 5 is populated with the values that you entered in the Readings window.
Select .
Note: If you do not supply a value in the Readings cell for all of the TMLs displayed in the grid, a confirmation message appears, indicating that one or more measurement values were not entered. The message asks you to confirm that you would like to continue saving.
The readings are saved.
For each reading that is saved, a Thickness Measurement is created and linked to the corresponding TML.
You can now recalculate the corrosion analysis.
Copyright © 1993-2015 Meridium, Inc. All rights reserved.