Add a Group with Permissions

The following instructions can be used to grant existing users permissions to a Public folder in the Catalog.

Note: No user can modify permissions to the Personal or Baseline folder.

Steps

  1. Access the Catalog page for the folder whose permissions that you want to modify.
  2. In the workspace heading, select , and then select Folder properties .

    The Catalog Folder Properties window appears, displaying the properties for the selected Catalog folder.

  3. Select Permissions.

    The Permissions section of the Catalog Folder Properties window appears displaying a grid that contains users and groups that have permissions to create, view, edit, or delete items within the selected folder.

  1. In the section heading, select .

    The Group Browser window appears.

  2. Select a group from the list, and then select Done.

    The selected group appears in the grid in the Permissions section of the Catalog Folder Properties window.

  3. Modify permissions for the group by selecting the check boxes and list options as necessary.
  4. Select Done.

    The selected group is granted permissions to the folder.

Copyright © 1993-2015 Meridium, Inc. All rights reserved.