The following instructions can be used to grant existing users permissions to a Public folder in the Catalog.
Note: No user can modify permissions to the Personal or Baseline folder.
In the workspace heading, select , and then select Folder properties .
The Catalog Folder Properties window appears, displaying the properties for the selected Catalog folder.
Select Permissions.
The Permissions section of the Catalog Folder Properties window appears displaying a grid that contains users and groups that have permissions to create, view, edit, or delete items within the selected folder.
In the section heading, select .
The User Browser window appears.
Select a user from the list, and then select Done.
The selected user appears in the grid in the Permissions section of the Catalog Folder Properties window.
Select Done.
The selected user is granted permissions to the folder.
Copyright © 1993-2015 Meridium, Inc. All rights reserved.