A query can be exported as a dataset, a fixed set of information that is stored as a Catalog item.
In the upper-right corner of the workspace, select , and then select Export to a Dataset.
The Save As window appears.
In the Name box, enter a name for the dataset. The name is required and must be unique to the Catalog folder in which you are saving the query.
The Caption box is populated automatically with the value that you entered in the Name box.
Select Save.
The dataset is saved to the Catalog.
Copyright © 1993-2015 Meridium, Inc. All rights reserved.