You can add either a parent Production Event Code or a Production Event Code that is the child of an existing parent.
Steps
In the Choose code box, select Production Event Codes.
The list of Production Event Codes appears.
To add a parent Production Event Code at the top level of the hierarchy, select
-or-
To add a child Production Event Code to an existing parent, select the check box next to the parent, and then select
The Add Production Event Code window appears.
Select
The Production Event Code is saved.
Copyright © 1993-2015 Meridium, Inc. All rights reserved.