Production Event Code Records

Production Event Code Records store details that represent a type of Production Event. This topic provides an alphabetical list and description of the fields that exist for the Production Event Code family and appear on the baseline Production Event Code datasheet. The information in the table reflects the baseline state and behavior of these fields.

Field Data Type Description Behavior and Usage
Code Character A short code that represents the type of event. This is a required field.
Color Character The color that is used to represent the production event code on the Production Data Summary graph.

This field contains a list, which displays all colors that you can assign to the impact code.

In the baseline database, colors are not assigned to the baseline Production Event Codes. You will need to assign the required colors manually.

Description Character A description of the type of event. You can define this field manually.

Copyright © 1993-2015 Meridium, Inc. All rights reserved.