Access and Modify the Dashboard Configuration

Steps

  1. Open an existing dashboard.

    -or-

    Create a new dashboard.

  2. In the upper-right corner of the page, select Edit Mode.

    Depending on your security permissions, the following options appear:

    Tip:  You can move widgets by selecting them and then dragging-and-dropping them in your desired location. You can also resize widgets by selecting the border of the widget and adjusting its dimensions.

  3. After making changes using the dashboard configuration options, select Edit Mode.

    The changes made to the dashboard are saved.

Copyright © 1993-2016 Meridium, Inc. All rights reserved.