Modify the Content of an Existing Widget

Steps

  1. Access the dashboard configuration options.
  2. In the upper-right corner of the widget that you want to modify, select, and then select Edit.

    The Edit Widget window appears, which contains configuration options that are specific to the widget type.

  3. Modify the properties of the widget as needed, and then select Save.

    The modified widget is saved.

Copyright © 1993-2016 Meridium, Inc. All rights reserved.