About the ACA Data Loader

The ACA Data Loader allows existing or new Asset Criticality Analyses to be delivered to the ACA module in Meridium Enterprise APM for further development, analysis or implementation. Customers will be able to load data from other external systems into the ACA module via the Excel workbook. They will be able to upload any existing analyses with updated risk assessment data that has been assessed outside the Meridium Enterprise APM application. Sites assignments for the ACA records that are loaded with the ACA Data Loader are inherited from the related Functional Locations and Equipment that already exist in the Meridium Enterprise APM system.

The data loader is used in the following scenarios:

Copyright © 1993-2016 Meridium, Inc. All rights reserved.