About the Hazards Data Loader

The Hazards Data Loader allows you to implement HAZOP Analysis when you have data in a legacy system that is not supported by Meridium Enterprise APM. To import data using the Hazards Data Loader, Meridium, Inc. provides an Excel workbook, Hazards.xlsx, which supports baseline Hazards Analysis in Meridium Enterprise APM. You must export your legacy system so that the data can be used to populate the workbook. The data from the workbook will then be imported into Meridium Enterprise APM using the Hazards Data Loader.

Note: The Excel template is referred to throughout this documentation as the data loader workbook.

The data loader workbook can be used in the following scenario:

After importing the data, the Hazards Data Loader creates the following records in Meridium Enterprise APM:

Note: This data loader workbook is not backward compatible to earlier versions of Meridium Enterprise APM.

There are two scenarios associated with modifications to the Hazards Data Loader:

Copyright © 1993-2016 Meridium, Inc. All rights reserved.