About the Production Loss Analysis (PLA) Data Loader

The Production Loss Analysis (PLA) Data Loader allows you to implement PLA when your production data exists in a legacy system. The Production Loss Analysis (PLA) Data Loader uses an Excel workbook, Production Loss Analysis (PLA).xlsx, as the source of data to be loaded into Meridium Enterprise APM. You must export your Production Data from your legacy system so that the data can be used to populate the data loader workbook. The data from the Excel workbook will then be imported into Meridium Enterprise APM using the Production Loss Analysis (PLA) Data Loader.

Note: The Excel workbook is referred to throughout this documentation as the data loader workbook.

The Production Loss Analysis (PLA) Data Loader can be used in the following scenarios:

After importing the data into Meridium Enterprise APM, you will be able to access Production Plans, view Production Data that is associated with the Production Plan, and view unaccounted losses and accounted losses that are associated with the production data details.

The data imported by the data loader allows you to maintain visibility and continuity in production reliability. The Production Loss Analysis (PLA) Data Loader creates the following records in Meridium Enterprise APM:

This data can be either forward facing (i.e., Production Plans that have production dates in the future) or backward facing (i.e., Production Plans in which production took place in the past).

Copyright © 1993-2016 Meridium, Inc. All rights reserved.