Steps
If, on the upper-left corner of the page, the <number> Error link appears beside the
Note: If the number of errors link does not appear, then the connections needed to use the data loaders are configured properly.
The Connection Errors screen appears displaying the connections status for each connection point need to use the data loaders.
Results
The connection status is tested. The following table describes the connection status for data import jobs.
Connection Test | Description | If you get an Error... |
---|---|---|
APM Connect Integration Web Services Test | Tests to see if the communication channels between the APM Connect server and the Meridium Integration web services are open. | Ensure the web services are running, and that port 80 is open. |
APM Connect Web API Test | Test the connection between Meridium Enterprise APM web API and the APM Connect server. | Ensure the ports are open between the Meridium Enterprise APM Serve and the APM Connect server. |
APM Connect Configuration Test | Test the configuration of the APM Connect connection parameters configured in Meridium Enterprise APM. | Ensure the parameters configured in Meridium Enterprise APM are correct to establish connection from Meridium Enterprise APM and APM Connect. |
APM Fileshare Access Test | Tests the file share system is connected to the Meridium Enterprise APM Server, so that the server can read and write to the configured file shares. | Ensure the parameters configured in Meridium Enterprise APM are correct to establish connection from Meridium Enterprise APM, and the user has the necessary permissions to access the file share. |
APM Staging Database Test | Tests the Meridium Enterprise APM Server is connected tot the APM Connect IR database. | Ensure that PostgresSQL is accepting the connection from Meridium Enterprise APM . These connections are managed in the file pg_hba.conf. |
APM Connect Fileshare Access Test | Tests the file share system is connected to the APM Connect server, so that the server can read and write to the configured file shares. | Ensure the parameters configured in Meridium Enterprise APM are correct to establish connection from Meridium Enterprise APM, and the user has the necessary permissions to access the file share. |
APM Connect Staging Database Test | Tests the connection between the APM Connect server and the IR database to ensure that files can read and written to the IR.. | Ensure the RunDataloadersRoute.cfg is configured correctly. |
Copyright © 1993-2016 Meridium, Inc. All rights reserved.