Delete a Sub Work Pack

Steps

  1. Access the Work Packs section.
  1. On the left side of the Work Packs section, select the Work Pack ID of the Work Pack whose Sub Work Pack you want to delete.

    The Work Pack Overview workspace for the selected Work Pack appears, displaying the Definitions section.

  1. In the left pane, select the Sub Work Pack that you want to delete.

    The workspace for the selected Sub Work Pack appears.

  2. In the left pane, select , and then select Delete.

    A message appears, asking you to confirm that you want to delete the selected Sub Work Pack.

  3. Select Yes.

    The Sub Work Pack is deleted. The Sub Work Pack and all of its associated records are deleted.

Copyright © 1993-2016 Meridium, Inc. All rights reserved.