Modify a Join's Properties

Steps: Modify a Meridium Join

  1. Access the Design workspace.
  2. On the design canvas, select the line that connects two query sources.

    The window for the selected relationship family appears.

  3. Select Join Properties.

    The Join Properties window appears.

  4. On the Join Properties window, modify the join type to one of the following options, and then select Done:

Steps: Modify a Manual Join

  1. Access the Design workspace.
  2. On the design canvas, select the line that connects two query sources.

    The Manual Join window appears.

  3. Select Join Properties.

    The Join Properties window appears.

  4. On the Join Propertieswindow, you can modify the predecessor and successor fields, and then change the join type to one of the following options. Then, select Done:

Copyright © 1993-2016 Meridium, Inc. All rights reserved.