A PRD Analysis is an analysis that contains data specific to pressure relief devices.
A PRD Analysis for a pressure relief device can be created once you have identified at least one piece of equipment or RBI Component that it protects. PRD Analyses function the same way as RBI Analyses.
However, the following features that are available for RBI Analyses are not available for RBI PRD Analyses:
When you create a Criticality Calculator PRD Component:
Criticality Calculator PRD Component - Relief Valve
Criticality Calculator PRD Component - Rupture Disk
Balanced Bellows PRD
Conventional PRD
Pilot-Operated PRD
PRD with Rupture Disk
Rupture Disk Only
An Equipment that represents a Pressure Relief Device cannot be linked to both RBI Components and PRD Components.