RBI Workflow

This workflow provides the basic, high-level steps for using this module. The steps and links in this workflow do not necessarily reference every possible procedure. For more procedures, see the links in the Related Information section.

The procedures for using RBI are organized into the following categories:

Risk Based Inspection Workflow

The steps and links in this workflow do not necessarily reference every possible procedure.

  1. Set up Corrosion Loops.
  2. Assign Degradation Mechanisms to each component.
  3. Create RBI Analyses.
  4. Analyze scenarios using a What If Analysis.
  5. Create Recommendations.