Create an RBI Criticality Analysis

Steps

  1. Access the RBI Component for which you want to create an RBI Criticality Analysis.
  2. Below the graph, select , and then select Semi-Quantitative (580).

    A new analysis is created, and the Analysis workspace for the new analysis appears, displaying the Analysis Details section.

    Note: When an analysis is created, the Consequence Evaluations and Degradation Mechanisms corresponding to the Potential Degradation Mechanisms linked to the selected component are also created.

  3. Enter values in the available fields.

  4. Review the required fields.
  5. In the upper-right corner of the section, select .

    The analysis is saved.