When you calculate an RBI
The unmitigated risk rank is plotted on a Risk Matrix. This value is the intersection of the consequence and probability that are calculated when you calculate an RBI
Consequence of Failure: The consequence of failure is the highest among the values in the following fields in the associated
Environmental Consequence Category
Note: The Environmental Consequence Category field contains a value only if the RBI Component contains the value Storage Tank - Bottom in the Component Type field.
Meridium Enterprise APM then locates the Risk Translation record with this temporary unmitigated risk value in the Source Risk Rank field and the value No (N) in the Financial? field.
The unmitigated financial risk rank is plotted on a Risk Matrix. This value is the intersection of the consequence and probability that are calculated when you calculate an RBI
Financial Consequence: The financial consequence is the highest among the values in the following fields in the associated
Product Leak Category
Note: The Product Leak Consequence field will contain a value only if the RBI Component contains the value Heat Exchanger - Bundle in the Component Type field.
Meridium Enterprise APM then locates the Risk Translation record with this temporary unmitigated risk value in the Source Risk Rank field and the value Yes (Y) in the Financial? field.