About Values Mapped to Risk

When you promote an asset to Asset Strategy Management (ASM), a Risk is created in ASM for each Degradation Mechanisms record (DM) in active RBI Criticality Analyses. This Risk contains the details of unmitigated and mitigated risks defined in the DM.

The following table provides a list of fields on the Risk datasheet that are populated from the DM or the associated RBI Criticality Analysis.

This Risk field:

...is populated with: ...from the following associated records:
Name

A value in the following format: <Equipment Description> ~ <Degradation Mechanism>

If there is no value in the Equipment Description field, then the value in the Equipment Type field is used.

RBI Criticality Analysis and DM

Description

A value in the following format: <Equipment Description> ~ <Degradation Mechanism>

If there is no value in the Equipment Description field, then the value in the Equipment Type field is used.

RBI Criticality Analysis and DM

Failure Mode The value in the Degradation Mechanism field DM
Maintainable Item A value in the following format: <RBI Component Entity ID> ~ <Equipment Description or Equipment Type> RBI Criticality Analysis and Criticality Calculator RBI Component
Failure Cause The value in the Degradation Mechanism field DM
Unmitigated Financial Risk The value in the Unmitigated Financial Risk Rank field DM
Risk Basis The value Risk Based Inspection